8 warnings in MQX/PE demo with TWRK60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8 warnings in MQX/PE demo with TWRK60

1,294件の閲覧回数
Kyle_Apollo
Contributor II

I got the bsp to compile with no problems, and installed both patches that were missing. 

 

For some reason, I am getting these 8 errors when I build the demo application, and I cannot figure out how to get rid of them.  

 

 

Any help would be greatly appreciated, thanks!

0 件の賞賛
返信
1 返信

1,071件の閲覧回数
petr_uhlir
NXP Employee
NXP Employee

The warnings which comes from multiple symbol definition in main.obj and bsp library (events.o) are OK. The default empty event functions which are generated by ProcessorExpert into events.c module are overloaded in pe_demo application in main.c module. The similar apply for isgraph and isupper symbols.

0 件の賞賛
返信