Hi Fred,
To run the demo you will need to build the following libraries for K60:
KSDK Platform Lib
C:\Freescale\KSDK_1.1.0\lib\ksdk_platform_lib\iar\K60D10
KSDK OSA for MQX Lib
C:\Freescale\KSDK_1.1.0\lib\ksdk_mqx_lib\iar\K60D10
MQX Lib
C:\Freescale\KSDK_1.1.0\rtos\mqx\mqx\build\kds\mqx_frdmk22f
MQX stdlib
C:\Freescale\KSDK_1.1.0\rtos\mqx\mqx_stdlib\build\iar\mqx_stdlib_twrk60d100m
MQX Shell Lib
C:\Freescale\KSDK_1.1.0\rtos\mqx\nshell\build\iar\nshell_twrk60d100m
RTCSLib
C:\Freescale\KSDK_1.1.0\tcpip\rtcs\build\iar\rtcs_twrk60d100m
You can import the library projects using the option in menu File > Import > General > Existing Project into Workspace
You can also import the 3 MQX Libs using the build_libs.wsd file with the option menu File > Import > Project of Projects > Existing project Sets. This working set is located in the following path:
C:\Freescale\KSDK_1.1.0\rtos\mqx\build\iar\workspace_twrk60d100m
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------