Hi All,
The new Freescale MQX™ 4.0.2.2 patch release is now available on the www.freescale.com.
· Files available
# | Name | Description |
1 | Freescale MQX RTOS 4.0.2.2 Patch | This patch release is based on the MQX™ RTOS 4.0.2 release and provides the solutions to software issues identified in the released version. This patch release applies to all the BSPs. |
· Patch Description
This patch provides the software workarounds for the following issues identified in MQX 4.0.2 release:
o ENGR00278434
§ Vybrid ARM Cortex®-A5: The float context is not properly saved when a task is blocked.
§ Affected BSPs: TWR-VF65GS10, AutoEVB Vybrid
o ENGR00273581
§ A memory allocation problem occurs when the system is out of memory.
§ Affected all BSPs
o ENGR00276466
§ Events are sometimes triggered immediately after they are added.
§ Affected all BSPs
o ENGR00279275
§ RTCS connect failures via Dell router
§ Affected all BSPs
· Known issues
o For known issues and limitations please consult the release notes document.