Now Available: MQX RTOS for Kinetis SDK v1.3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Now Available: MQX RTOS for Kinetis SDK v1.3.0

Now Available: MQX RTOS for Kinetis SDK v1.3.0

We are pleased to announce the release of MQX RTOS for Kinetis SDK v1.3.

Boards Supported

FRDM-K22F

FRDM-K64F

FRDM-KL46Z

FRDM-KW24

FRDM-KL43Z

FRDM-KL27Z

FRDM-KL25Z

FRDM-KL26Z

USB-KW24D512

MRB-KW01

TWR-K22F120M

TWR-KV31F120M

TWR-K24F120M

TWR-K64F120M

TWR-KV10Z32

TWR-K60D100M

TWR-KL46Z

TWR-K21D50M

TWR-K21F120M

TWR-KW24D512

TWR-KL43Z48M

TWR-K65F180M

New Features and Updates

  • MQX RTOS - version 5.0.3 Updates
    • MQX RTOS Kernel has been updated to address several issues related to the task restart and the timer component
  • RTCS - version 4.2.0 Updates
    • The CyaSSL 3.3.0 was upgraded to the WolfSSL version 3.4.6. The location of the library was changed from the middleware/tcpip/rtcs/source/ssl to the middleware/security/wolfssl. The library usage is demonstrated in the
      middleware/tcpip/rtcs/examples/httpsrv example application.
  • Other Updates
    • Added two example applications demonstrating the Kinetis cryptography capabilities - WolfSSL crypto library benchmark : \examples\<board>\demo_apps\security\benchmark_wolfssl

How to Get Started

Note: As of Kinetis SDK v1.2, MQX RTOS components are available in the Kinetis SDK itself.

1. Visit http://www.freescale.com/ksdk

2. Click Download

2015-05-11 16_07_38-Freescale MQX™ Software Solutions_Freescale.png

3. Click KSDK v1.3.0 Mainline Release

pastedImage_18.png

4. Review and click to agree to the license terms if they are acceptable.

pastedImage_19.png

5. Click and installer for your Host OS.

6. Download and Install.

On Windows, the default source installation directory is C:\Freescale\KSDK_1.3.0

7. Check out the getting started guides in the /docs directory.

Enjoy!  Best of luck with your embedded projects!

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎10-19-2015 08:10 PM
更新者: