How To: Porting MQX RTOS v4.x to MQX RTOS for KSDK v1.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How To: Porting MQX RTOS v4.x to MQX RTOS for KSDK v1.2

How To: Porting MQX RTOS v4.x to MQX RTOS for KSDK v1.2

Hi,

Check out this new porting guide.  It includes information on paths and project configurations in MQX RTOS for Kinetis SDK v1.2.

Porting an MQX RTOS Application to MQX RTOS for Kinetis SDK

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/MQXKSDKPUG.pdf?fpsp=1&WT_TYPE=Users...

Contents

1 Introduction ....................................................................... 1
2 Why port?..........................................................................  2

3 What is different in the new Kinetis SDK-based

   architecture? ......................................................................2

4 Overview of porting application.......................................... 5

5 Porting the Application....................................................... 6

6 Conclusion ...................................................................... 28

コメント

The paths for RTCS are out of date, as they appear to have been moved to a "middleware" folder for 1.2.0.

I would very much appreciate some more info on "how to add RTCS to your MQX project."  These notes say it is no different than it was before, but there was no documentation before either (except to link the static lib and hope for the best).

Thanks!

Hi,

Thanks for the feedback. 

You might  want to check out lab 4 in the training Training Class: MQX RTOS for Kinetis SDK, Kinetis Design Studio (6 labs, including TCP/IP)

The examples should give a good overview of adding and using RTCS to a project.

Thanks,
Mac

評価なし
バージョン履歴
最終更新日:
‎05-13-2015 12:22 PM
更新者: