which trace32 debugger is best for MPC577C MCU using S32 IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

which trace32 debugger is best for MPC577C MCU using S32 IDE

Jump to solution
2,738 Views
vrushalitaklika
Contributor III

I am looking for bet fit debugger for MPC5777C MCU.

I have narrowed own to trace32. however need more clarification if both these trace32 are required.

Jtag Debugger   
Descriptionorder/part no.NameFunctionality
Host InterfaceLA-3500Power Debug ProUniversal debug controller with USB 3.0 for Windows/Linux/MacOSX 
Connector adapterLA-3736JTAG Debugger for MPC5xxx Automotive  supports Qorivva MPC5xxx/SPC5xxx (e200 cores)
and Freescale PX SERIES processors
eTPU, GTM and SPT debugging included

Thanks

Vrushali

1 Solution
2,380 Views
fraidling
Contributor II

Hello Vrushali,

we use a similar setup for Debugging the MPC5777C. (Edit: same Setup as Peter)

You need a Power Debug Interface USB 2.0/USB 3.0 (LA-3500) and an architecture specific debug cable, for MPC5XXX the LA-3736.
The Trace 32 License is programmed on the debug cable, for multi-core debugging you also need the LA-7960X license.

Florens

View solution in original post

2 Replies
2,381 Views
fraidling
Contributor II

Hello Vrushali,

we use a similar setup for Debugging the MPC5777C. (Edit: same Setup as Peter)

You need a Power Debug Interface USB 2.0/USB 3.0 (LA-3500) and an architecture specific debug cable, for MPC5XXX the LA-3736.
The Trace 32 License is programmed on the debug cable, for multi-core debugging you also need the LA-7960X license.

Florens

2,380 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I am using LA-7708 body and LA-7753R cable.

I expect that LA-3500 and LA-3736 are new version of what I am using. I see no issue here.

Peter

0 Kudos
Reply