where is MPC5745R?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where is MPC5745R?

778件の閲覧回数
merlinz
Contributor II

I'm looking at this microcontroller but I do not know what is the correct information. In the title indicates that it has 3MB and 3 core and 200mhz but in its description does not put the same, in the datasheet specifies it in different way and in the reference manual it say 150mhz for mpc5745r.

I can not find the MPC5745R for sale, maybe it is now called mpc5743r in 176?

Actually the one that suits me the most is the MPC5745R in 176TQFP, but I can not find it anywhere, it is not manufactured anymore. or has it changed its name?

BasicType 

SPC5743RK1MLU5(Active)

NXP 32-bit MCU, Triple Power Arch core, 3MB Flash, 200MHz, -40/+125degC,Automotive Qual,LQFP17

タグ(2)
0 件の賞賛
2 返答(返信)

620件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I recommend you to use MPC5743R in 176 pin package as it is available.

But if you need MPC5745R I am sure we can manufacture it on request of reasonable amount. But this will take some time. I expect long time.

Basically customers use MPC5746R or MPC5743R.

Peter

620件の閲覧回数
merlinz
Contributor II

Thanks for the information, I will keep it in mind.

0 件の賞賛