we are using the SPC5606S chip and I want the example procedure especially for the TFTdriving

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

we are using the SPC5606S chip and I want the example procedure especially for the TFTdriving

548 Views
jiangyu
Contributor II

we are using the SPC5606S  chip  and I want the example  procedure especially for the TFTdriving. Thanks for your kind answer.

4 Replies

418 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, do you have MPC5606S-DEMO-V2 evaluation board?

418 Views
jiangyu
Contributor II

Thanks for your answer. We don't have the evaluation board ,but we have made the evaluation board(PCB) by ourself. And now we are aimed to develop the new product ,so we need the example procedure for TFT urgently. Best wishes for you.

0 Kudos

418 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you had MPC5606S-DEMO-V2 board, there is CD in the package containing graphics driver. It is however not for download on our web.

However it you start from scratch you will at beginning deal with TFT connection.

If you create new case (mention this thread number to the subject) I could send the driver and MPC5606S-DEMO-V2:

How to submit a new question for NXP Support 

Also you could see for instance here:

Dashboard Cluster Demo - MPC5606S | Axiom Manufacturing 

Check application notes for MPC5606S and MPC5645S devices:

MPC560xS|32-bit MCU|Instrument Clusters|NXP 

MPC564xS|32-bit MCU|Instrument Clusters|NXP 

Hope it helps

418 Views
jiangyu
Contributor II

waiting for your answers.

0 Kudos