the problem to use eQADC in MPC5644A, how to use 2 channels together

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the problem to use eQADC in MPC5644A, how to use 2 channels together

Jump to solution
1,161 Views
xushengyu
Contributor II

dear, all.

I do not know how to use eQADC normally, i want to use 2 ADC channels together, but i have no idea to configure it correctlly. For example, i want to use AN6 and AN22 together. Here is my codes, but it can not work,

0 Kudos
1 Solution
934 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, following example code shows simultaneous conversion of two channels. If is given by targeting of command into CBuffer0 or CBuffer1 which also specify used A/D converter. The example is written for different device using the same ADC.

Example MPC5674F eQADC+eDMA Single_Scan CW210 

As start point you may use following one I have written for MPC5644A:

https://community.nxp.com/docs/DOC-101791 

pastedImage_4.png

pastedImage_7.png

pastedImage_5.png

pastedImage_6.png

View solution in original post

0 Kudos
1 Reply
935 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, following example code shows simultaneous conversion of two channels. If is given by targeting of command into CBuffer0 or CBuffer1 which also specify used A/D converter. The example is written for different device using the same ADC.

Example MPC5674F eQADC+eDMA Single_Scan CW210 

As start point you may use following one I have written for MPC5644A:

https://community.nxp.com/docs/DOC-101791 

pastedImage_4.png

pastedImage_7.png

pastedImage_5.png

pastedImage_6.png

0 Kudos