s32ds Spi transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32ds Spi transfer

623件の閲覧回数
bharathn3402
Contributor II

Screenshot 2024-04-12 143415.png

here i have two slaves are connected to an single chipselect pin. Iam not sure how to communicate with the slave devices individuallly. can anyone help me out in this?
#spi

#s32ds

タグ(2)
0 件の賞賛
返信
4 返答(返信)

607件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you want to use additional chip selects then you have to route the pin for it in the pin_mux component and generate PE code. Then before calling Master transfer function you can switch CS using DSPI_UpdateCS function.
This function can be used to change the chip select configured when the driver was initialized. It is useful for applications where more slave devices are controlled by only one DSPI/SPI instance.

BR, Petr

0 件の賞賛
返信

603件の閲覧回数
bharathn3402
Contributor II
Hi petrs,
My question was i have connected two devices to an an single chipselect pin. how can we communicate with both devices whenever i want?
0 件の賞賛
返信

599件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should not have connected more slaves to same single chip select. How do you then deal with slaves SOUT signals connected to MCU SIN input?

BR, Petr

0 件の賞賛
返信

535件の閲覧回数
bharathn3402
Contributor II

HI
i have connected multiple CSB pins to an single dspi chipselect output how to switch between two csb pins in software whenever we want?
in my case for chipselect 3 i  have connected two csb pins. some times i want to communicate with pd3 and some times i want to communicate with the pf5. how?
Screenshot 2024-04-12 143415.png

タグ(2)
0 件の賞賛
返信