phy_autoneg on MPC5748G LCEVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

phy_autoneg on MPC5748G LCEVB

跳至解决方案
1,306 次查看
karma_JC
Contributor I

Hi:

Working on PHY driver using example phy_autoneg example.    Base on my assumption, the cable unplug/plug should call one of action(Link up, Link down, autoneg complete, and autoneg failed) callback.  However, those action-callbacks could not be reached when I unplug/plug cable from the ethernet port on MPC5748G LCEVB.  I checked the configuration on ENET(ENET0, MII), and PHY being pointing at the configuration of ENET0.  So, the configuration shall be good.  I traced the the code a  little from mainFunciton->PHY_Read->readC122->ENET_DRV_MDIORead.  The value readback after masking is always 0xFFFF regardless cable being plug in to the port or not.  Will this "phy_autoneg" example work on MPC5748G LCEVB board????

Thanks

James

0 项奖励
回复
1 解答
1,283 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

example was done for DEVKIT board, however will be running for LCEVB too after some modification. DEVKIT is using RMII connection , LCEVB MII connection.
PA7 and PA10 pins are used to drive LEDs on example and it is connected to PHY outputs on LCEVB, so at least you should unroute pins in pin_mux component.
Then PHY is using address 1 so you need to change it in PHY component

PetrS_0-1651141433042.png

Then it should work on LCEVB.

Ideally change config to MII mode and add rest of MII signals in pinmux and also config pins for LEDs and modify used code to drive right pins for LEDs .

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,270 次查看
karma_JC
Contributor I

Hi PetrS:

I've resolved this by finding out the default PHY address of TI DP83848C being set to 1.  The problem has been resolved.

Thank you

James

0 项奖励
回复
1,284 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

example was done for DEVKIT board, however will be running for LCEVB too after some modification. DEVKIT is using RMII connection , LCEVB MII connection.
PA7 and PA10 pins are used to drive LEDs on example and it is connected to PHY outputs on LCEVB, so at least you should unroute pins in pin_mux component.
Then PHY is using address 1 so you need to change it in PHY component

PetrS_0-1651141433042.png

Then it should work on LCEVB.

Ideally change config to MII mode and add rest of MII signals in pinmux and also config pins for LEDs and modify used code to drive right pins for LEDs .

BR, Petr

0 项奖励
回复