[mpc5777c] Can't I use e_stw to initialize SRAM ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[mpc5777c] Can't I use e_stw to initialize SRAM ?

Jump to solution
1,118 Views
jaejynshin
Contributor III

Hello Expert

I want to initialize SRAM which has ECC error using e_stw. Because I want to clear a few bytes of Ram memory.

But there was a Exception when I used e_stw.

sram_init_some:
    e_lis r5, SOME_RAM_SIZE@h # Initialize r5 to size of SRAM (Bytes)
    e_or2i r5, SOME_RAM_SIZE@l
    # e_srwi r5, r5, 0x6
    mtctr r5

    # Set Base Address of the internal SRAM
    e_lis r5, SOME_RAM_START@h
    e_or2i r5, SOME_RAM_START@l

sram_init_some_loop:
    e_stw r16,0(r5)
    e_addi r5,r5,4
    e_bdnz sram_init_some_loop

Can't I use e_stw to init SRAM?

I can't, how to initialize a few bytes of SRAM ? (not 64 bytes using e_stmw)

Thank you

Jaejyn

1 Solution
895 Views
jaejynshin
Contributor III

I resolved it.

I used e_stmw and r30/r31 register.

I set the resolution of clearing size as 8 bytes.

Thank you anyway.

View solution in original post

2 Replies
895 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

As there is ECC protection on SRAM the operation executed is read-modify-write.

So you have to use stmw.

Peter

896 Views
jaejynshin
Contributor III

I resolved it.

I used e_stmw and r30/r31 register.

I set the resolution of clearing size as 8 bytes.

Thank you anyway.