Hi, I am using mpc #5674f and I have to work with #SPI peripheral in it. If I successfully initiate SPI and be able to transmit / receive data with it, I'm gonna use it in my #RTC project.
Then I send the command with PUSHR register, then check Transmit Complete Flag and read it with POPR.
Can anyone help me?
Thank you in advance.
Regards.
Ceren.
Hi, I could recommend you to try to see following example. Theoretically you could run directly with MPC5674F device as it is compatible with MPC5676R:
https://community.nxp.com/docs/DOC-335461
It configures DSPI module for very slow communication (example communicates with external memory), you could see some traffic on SPI communication lines.