#include "netifcfg.h" file not found error in MPC5748G: ENET_PING example.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

#include "netifcfg.h" file not found error in MPC5748G: ENET_PING example.

3,497 Views
tejo2one
Contributor III

Hello,

 

I am working on NXP Gateway board which uses MPC5748G, I need to setup Ethernet communication and checking example codes. ENET_PING : found this example code but it doesnot build. Is there any example code using ethernet interface which works using MPC5748G.

Thank you in advance,

Tejo

tejo2one_0-1680545653829.png

 

0 Kudos
Reply
10 Replies

3,470 Views
tejo2one
Contributor III

Thanks for the response Lukas.

I apologize for mistake, I am using example "lwip_mpc5748g" not ENET_PING.

tejo2one_0-1680797030190.png

 

0 Kudos
Reply

3,464 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Exactly the same is working also for lwip example. Can you find the file in S32DS folder? Isn't the installation corrupted?

Regards,

Lukas

0 Kudos
Reply

3,458 Views
tejo2one
Contributor III

I uninstalled and reinstalled S32DS., still same issue.

Can you share your code ?

0 Kudos
Reply

3,462 Views
tejo2one
Contributor III
Lucas, I could not find this file.
For my reference what is the S32DS version you're using?
0 Kudos
Reply

3,407 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @tejo2one 

I used S32DS 2.1 and SDK 3.0.3.

I just found out that the file is not present in the S32DS installation folder but it's generated by processor expert, so I can see it in my project.

I will attach my project here, you can try to import it.

Regards,

Lukas

0 Kudos
Reply

3,171 Views
tejo2one
Contributor III

Hello @lukaszadrapa ,

              Thanks for your code. I tried loading it in as a local project and when I give generate code command "netifcfg.c and netifcfg.h" are removed by tool.

               I felt my tool was corrupted so reinstalled S32DS again but same problem still exists.

Is there any link where I can download whole setup locally and install it? please support me its already taken lot of time.

 Thanks in advance.

Tejo

 

0 Kudos
Reply

3,159 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @tejo2one 

If you go to:

Help -> S32DS Extensions and Updates

and

Help -> About S32 Design Studio... -> Installation Details

... could you see if all these packages are installed? That's my setup which works:

lukaszadrapa_0-1683022143328.png

 

lukaszadrapa_1-1683022152941.png

There's no way to install this as a one single package.

Regards,

Lukas

0 Kudos
Reply

3,381 Views
tejo2one
Contributor III

Hello Lukas,

 

Thanks for reply and code. I tried flashing your code but its stuck in HSM_Init during SSL_Init.

Is HSM firmware required to use TCPIP stack ?

 

Thanks & best regards,

Tejo

0 Kudos
Reply

3,374 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Please take a look at this thread:

https://community.nxp.com/t5/MPC5xxx/WolfSSL-on-MPC5748G-devkit/m-p/1460985

And also this one - it is possible to use SW implementation only:

https://community.nxp.com/t5/S32-SDK/using-wolfSSL-library-on-MPC5748G-board-with-out-HSM-firmware/m...

Regards,

Lukas

0 Kudos
Reply

3,472 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @tejo2one 

I can see no problem on my side. What I did:

File -> New -> S32DS Project from Example

Then I selected mentioned enet_ping example for MPC5748G.

Now the key point - it is necessary to generate the code by this:

lukaszadrapa_2-1680794091400.png

Or select in main menu: Project -> Generate Processor Expert Code.

Then you should be able to build the project.

Regards,

Lukas

 
0 Kudos
Reply