how to set more than one input Trigger source on Cross-Triggering Unit (CTU)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to set more than one input Trigger source on Cross-Triggering Unit (CTU)?

666 Views
834981225
Contributor I

Hi!

      I choose the  Trigger source from ETIMER0_IN and the PWM_ODD ,but it can only to implement  a Trigger.

0 Kudos
3 Replies

559 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Input trigger signals are ORed.

pastedImage_1.png

As there is only 1 TGS you can only have 1 reaction on the input trigger.

I am not able to understand from your description what you are trying to achieve.

Peter

0 Kudos

559 Views
834981225
Contributor I

Peter

        Hi,Thank's your answer.I'm trying  to implement  two input trigger signals that is not happen on the same time,and then i can get data of the

ADC channel when a corresponding input trigger was happened.

0 Kudos

559 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

If the signals are synchronous then it is possible to use CTU for 2 input triggers.

You just have to arrange 2 ADC command list to do so. ADC command list is double buffered and are updated on MSR.

it will looks like:

pastedImage_2.png

Peter

0 Kudos