help with custom board based on mpc5200b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

help with custom board based on mpc5200b

979 Views
lorenzoforzini
Contributor I

Hello, we're using a custom board based on mpc5200b

 

We are using kernel 2.6.33 and when we using ethernet, we get 80% packet loss with ping.

Where could i find the solution?


 

U-boot information:

CPU:   MPC5200B v2.2, Core v1.4 at 132 MHz

      Bus 132 MHz, IPB 132 MHz, PCI 66 MHz

Board: Ran Controller Board

 

I2C:   85 kHz, ready

 

Thanks


 

Lorenzo

Labels (1)
Tags (2)
3 Replies

705 Views
rameshchandraka
Contributor III

Dear Lorenzo

I want to migrate from kernel 2.6.16 to any newer working (kernel 2.6.28 ) one for my

lite 5200b board. pls suggest

---Ramesh

0 Kudos

705 Views
rameshchandraka
Contributor III

Dear all

I have u-boot latest version with latest kernel (3.5.x)

it is working fine...

Enjoy the Device tree concepts...was introduced...

Power PC with latest kernel power...Ever Green..

Thanks all

--Ramesh

0 Kudos

705 Views
lorenzoforzini
Contributor I

Now i'm thinking that one of main problem is 1:1 cpu:bus ratio, is possible?

Thanks

Lorenzo

0 Kudos