freeRTOS on SDK_RTM3_0_0 for MPC574x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freeRTOS on SDK_RTM3_0_0 for MPC574x

1,444 Views
zhaoyanling
Contributor III

Dear expert:

I development On DEVKIT-MPC5748G board, and I use SDK_RTM_3_0_0, I have add the file path, but there is an error, shown as following. How can I resolve the problem? Can you help me?

error1.jpg

SDK_version.jpg

path.jpg

Tags (2)
0 Kudos
Reply
3 Replies

1,377 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

did you generate PE code again once you added FreeRTOS component

pastedImage_1.png

The file is then located in Generate Code folder

BR, Petr

0 Kudos
Reply

1,377 Views
zhaoyanling
Contributor III

Hallo Petr Stancik,

Thank you very much for your reply.

Yes , PE codes are generated, shown as following. What may be the other reasons? 

generated.jpg

0 Kudos
Reply

1,377 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

so you generated PE code, then built the project again and error still appears, weird.

Not sure, check paths, clear errors manually in Problems window, clean project and build it once again.

BR, Petr  

0 Kudos
Reply