Dear expert:
I development On DEVKIT-MPC5748G board, and I use SDK_RTM_3_0_0, I have add the file path, but there is an error, shown as following. How can I resolve the problem? Can you help me?
Hi,
did you generate PE code again once you added FreeRTOS component
The file is then located in Generate Code folder
BR, Petr
Hallo Petr Stancik,
Thank you very much for your reply.
Yes , PE codes are generated, shown as following. What may be the other reasons?
so you generated PE code, then built the project again and error still appears, weird.
Not sure, check paths, clear errors manually in Problems window, clean project and build it once again.
never-displayed