flashing with bin2hex conversion file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

flashing with bin2hex conversion file

跳至解决方案
1,234 次查看
bjrajendra
Senior Contributor I

Hello all,

I'm using MPC5602P on CW2.9 platform. I wanted to know what will happen if I flash the unused bytes with 0x00 instead of 0xFF. The reason why I'm asking is, after my bin2hex conversion all my unused bytes are filled with 0x00 but not 0xFF. Also I don't want to use direct mot or hex file. Kindly help.

Thanks in advance,

BJ Rajendranath

0 项奖励
回复
1 解答
1,133 次查看
bjrajendra
Senior Contributor I

Nothing happens. You can still flash with 0x00 and the code will work as expected.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,134 次查看
bjrajendra
Senior Contributor I

Nothing happens. You can still flash with 0x00 and the code will work as expected.

0 项奖励
回复