etpu,mpc5775b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

etpu,mpc5775b

Jump to solution
689 Views
Fly213
Contributor II

Hi everyone:

I want to use etpu module to collect pwm,
But when I reuse the pin as etpu, my pin input is close to 0V (pwm with a peak value of 400mV), which was originally a peak value of 3.36V V..
I'm not sure what happened, so I'll ask you for help. If possible, please share an eTPU capture routine suitable for mpc5775.

Thanks,

Best Regards

Tags (1)
0 Kudos
Reply
1 Solution
648 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

my pin input is close to 0V (pwm with a peak value of 400mV), which was originally a peak value of 3.36V V..

This is a bit strange as MPC5775B does not have an eTPU module.

petervlna_0-1686634650966.png

best regards,

Peter

PS: I have check with eTPU expert an no example code is available for capture function.

 

View solution in original post

0 Kudos
Reply
2 Replies
649 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

my pin input is close to 0V (pwm with a peak value of 400mV), which was originally a peak value of 3.36V V..

This is a bit strange as MPC5775B does not have an eTPU module.

petervlna_0-1686634650966.png

best regards,

Peter

PS: I have check with eTPU expert an no example code is available for capture function.

 

0 Kudos
Reply
640 Views
Fly213
Contributor II
Thank you very much for your reply,
I was curious why my processor expert didn't have the configuration of eTPU, so I used the program of 5775e, but why can I use the eTPU program of 5775e to output pwm at 5775b?
There may be a problem here that I can't understand, but it doesn't matter.
Thank you again for your reply, which makes me not dwell on it any more.
0 Kudos
Reply