error while storing C_PowerOffDelayTime to CALI_flash with smpu configration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error while storing C_PowerOffDelayTime to CALI_flash with smpu configration

832件の閲覧回数
steven_zhang
Contributor V

问题:程序中读取 C_PowerOffDelayTime,其放在 FLASH 区域 cali_flash,在使用 smpu 配置

后,出现 bus_error 错误,请问哪里设置有问题?

there is  an error while storing C_PowerOffDelayTime to CALI_flash with smpu configration,is the configration ok in the attachment file.

0 件の賞賛
返信
1 返信

823件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

This is not correct:

lukaszadrapa_0-1642437860690.png

WORD1 is not size. WORD1 is end address which must be higher than start address.

lukaszadrapa_1-1642437929167.png

Regards

Lukas

0 件の賞賛
返信