error while storing C_PowerOffDelayTime to CALI_flash with smpu configration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

error while storing C_PowerOffDelayTime to CALI_flash with smpu configration

890 次查看
steven_zhang
Contributor V

问题:程序中读取 C_PowerOffDelayTime,其放在 FLASH 区域 cali_flash,在使用 smpu 配置

后,出现 bus_error 错误,请问哪里设置有问题?

there is  an error while storing C_PowerOffDelayTime to CALI_flash with smpu configration,is the configration ok in the attachment file.

0 项奖励
回复
1 回复

881 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

This is not correct:

lukaszadrapa_0-1642437860690.png

WORD1 is not size. WORD1 is end address which must be higher than start address.

lukaszadrapa_1-1642437929167.png

Regards

Lukas

0 项奖励
回复