eTPU2 set

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eTPU2 set

1,297件の閲覧回数
208677262
Contributor II

关于eTPU FUEL 设置多次喷油脉宽。

我在AN4907 文档中看到 FUEL里有这么一句话  The CPU can update the amount of injected fuel anytime using the function fs_etpu_fuel_update_injection_time(),which not only sets the injection_time value for the next engine cycles, but also updates the current injection - shorts the pulse, extends the pulse or generates an additional pulse.

打开 fs_etpu_fuel_update_injection_time() 函数,里面只有设置  injection_time ,请问 extends the pulse or generates an additional pulse 该如何设置?

0 件の賞賛
3 返答(返信)

1,206件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, would you please translate this question to the English? Thanks

0 件の賞賛

525件の閲覧回数
Wanglu
Contributor II
I want to adjust the hold current hold time to 2min, or more. How to adjust?
0 件の賞賛

1,206件の閲覧回数
208677262
Contributor II

Hi, I had a problem debugging eTPU. 

I checked the FUEL in AN4907 document, which said that the extra pulse width could be set through the fs_etpu_fuel_update_injection_time() function. But I checked that the function had only set the pulse width time. I wanted to know how to set the pulse width multiple times with FUEL.

Look forward to your reply.

0 件の賞賛