eTPU2 division with Freescale C compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eTPU2 division with Freescale C compiler

731 Views
RDH75
Contributor I

I am working on programming the eTPU2 peripheral for the MPC5644A, and I am receiving a linker error.

 

When I add a simple division statement in C (for example:  variable_a = variable_b / variable_c) I receive the following error:

 

 

#Error: could not locate symbol '__s32_div_f', required through section...

 

Looks like a runtime library is required, or something.  I cannot find any documentation on runtime libraries with the Freescale eTPU C Compiler.  If anyone knows the solution please help.  Thanks.

Labels (1)
Tags (2)
1 Reply

485 Views
stanish
NXP Employee
NXP Employee

Hello Randall,

Since eTPU doesn’t have signed division instruction, we provide signed division as a library file.

You should include the lib.c file as part of  your build.

You can find the library file from eTPU installation directory at : <CW for ETPU v10.x>\ETPU\ETPU_Tools\Command_Line_Tools\lib

Hope it helps.

Stan