eDMA issue on MPC5746R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eDMA issue on MPC5746R

420 Views
qm1013
Contributor III

Hello, About eDMA module.DMA_TCDn_WORD_2_MLOOP.jpg

There is the MLOFF field in the DMA_TCDn_WORD_2_MLOOP register. But I can't find the MLOFF in the pseudo-code steps of channel processing. Bellow is the ending minor loop.TIM截图20190617171039.jpg

How it affect the processing when it is enable ?

Labels (1)
Tags (1)
0 Kudos
1 Reply

381 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

MLOFF will create minor loop offset.

When minor loop offsets are enabled, the minor loop offset (MLOFF) is added to the final source address (SADDR), or the final destination address (DADDR), or both prior to the addresses being written back into the TCD.

regards,

Peter

0 Kudos