ds13 (3v3 volt led) is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ds13 (3v3 volt led) is not working

303 Views
turkmani_11
Contributor III

hi , i was debugging my mpc5748G and suddenly it stopped working and when i debug again it gives me the following,

turkmani_11_0-1668596127295.png

my j11 is on 2-3 but the 3V3 led stopped working only the 5V led is working, how can i solve this problem?

Tags (2)
0 Kudos
1 Reply

291 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

without functional 3.3V supply the MCU will not work. So try both USB and external 12V supply option and measure both 5V and 3.3V supplies (for example on J13 header). If there is no or low voltage on 3.3, most probably a 3.3V Switching Regulator will be wrong.

BR, Petr

0 Kudos