ds13 (3v3 volt led) is not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ds13 (3v3 volt led) is not working

286件の閲覧回数
turkmani_11
Contributor III

hi , i was debugging my mpc5748G and suddenly it stopped working and when i debug again it gives me the following,

turkmani_11_0-1668596127295.png

my j11 is on 2-3 but the 3V3 led stopped working only the 5V led is working, how can i solve this problem?

タグ(2)
0 件の賞賛
1 返信

274件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

without functional 3.3V supply the MCU will not work. So try both USB and external 12V supply option and measure both 5V and 3.3V supplies (for example on J13 header). If there is no or low voltage on 3.3, most probably a 3.3V Switching Regulator will be wrong.

BR, Petr

0 件の賞賛