dmpc5777c seral boot loader and RAppID Boot Loader Utility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dmpc5777c seral boot loader and RAppID Boot Loader Utility

723 Views
Alex5080
Contributor II

when I use RAppID Boot Loader Utility to dowload application. there is message is as attached picture.

on target board side,    use eSCI_A as boot serial . EVTO PIN is float. Bootcfg set as 01.

the error message told that  we should use CAN interface not serial(232) interface. In fact, we used uart (232) not CAN inteface.

Would you  please help to check it ? 

0 Kudos
Reply
2 Replies

717 Views
stanish
NXP Employee
NXP Employee

Hello Alex,

Just to better understand your setup: 

Have you downloaded .rbf file into your board first via JTAG?

RAppid BL does not support BAM "Hardware boot" for MPC57xx so BAM setup has no effect whatsoever.

Which board are you targetting - custom one of NXP EVB?

Stan

 

0 Kudos
Reply

705 Views
Alex5080
Contributor II
1. don't download rbf file via JTAG. 2.target board is customer board. not NXP even board. 3. use eSCI_A as boot serial. 4. bootcfg configure as 01.
0 Kudos
Reply