about AIPS for UART DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about AIPS for UART DMA

2,049件の閲覧回数
xinweichang
Contributor III

I am now using 5748G EVB to write a UART DMA demo. I noticed that a similar demo on 5744p there is AIPS_A_init() and AIPS_B_init(). But I don't quite know how to use this module. Is it the same on  5748GEVB?  Here is the code for 5744P.

 

void AIPS_A_Init(void)
{
    // All Master Can go through AIPS_A and all peripheral have no protection

    // Master Privilege Register A

AIPS_A.MPRA.R      = 0x77777777;
    // Peripheral Access Control Register
    AIPS_A.PACR[0].R    = 0x0;
    AIPS_A.PACR[1].R    = 0x0;
    AIPS_A.PACR[2].R    = 0x0;
    AIPS_A.PACR[3].R    = 0x0;
    //AIPS_A.PACR[4].R    = 0x0; - Reserved, not implemented
    AIPS_A.PACR[5].R    = 0x0;
    AIPS_A.PACR[6].R    = 0x0;
    AIPS_A.PACR[7].R    = 0x0;

    // Off-Platform Peripheral Access Control Register
    AIPS_A.OPACR[0].R = 0x0;
    AIPS_A.OPACR[1].R = 0x0;
    AIPS_A.OPACR[2].R = 0x0;
    AIPS_A.OPACR[3].R = 0x0;
    AIPS_A.OPACR[4].R = 0x0;
    AIPS_A.OPACR[5].R = 0x0;
    AIPS_A.OPACR[6].R = 0x0;
    AIPS_A.OPACR[7].R = 0x0;
    AIPS_A.OPACR[8].R = 0x0;
    AIPS_A.OPACR[9].R = 0x0;
    AIPS_A.OPACR[10].R = 0x0;
    AIPS_A.OPACR[11].R = 0x0;
    AIPS_A.OPACR[12].R = 0x0;
    AIPS_A.OPACR[13].R = 0x0;
    AIPS_A.OPACR[14].R = 0x0;
    AIPS_A.OPACR[15].R = 0x0;
    AIPS_A.OPACR[16].R = 0x0;
    AIPS_A.OPACR[17].R = 0x0;
    AIPS_A.OPACR[18].R = 0x0;
    AIPS_A.OPACR[19].R = 0x0;
    AIPS_A.OPACR[20].R = 0x0;
    AIPS_A.OPACR[21].R = 0x0;
    AIPS_A.OPACR[22].R = 0x0;
    AIPS_A.OPACR[23].R = 0x0;
    AIPS_A.OPACR[24].R = 0x0;
    AIPS_A.OPACR[25].R = 0x0;
    AIPS_A.OPACR[26].R = 0x0;
    AIPS_A.OPACR[27].R = 0x0;
    AIPS_A.OPACR[28].R = 0x0;
    AIPS_A.OPACR[29].R = 0x0;
    AIPS_A.OPACR[30].R = 0x0;
    AIPS_A.OPACR[31].R = 0x0;
}

/*******************************************************************************
Function Name : AIPS_B_Init
Engineer      : Martin Kovar
Date          : Dec-16-2015
Parameters    : NONE
Modifies      : NONE
Returns       : NONE
Notes         : Setup access right for Masters and Peripherals on AIPS
Issues        : NONE
*******************************************************************************/
void AIPS_B_Init(void)
{
    // All Master Can go through AIPS_B and all peripheral have no protection

    // Master Privilege Register A
    AIPS_B.MPRA.R      = 0x77777777;
    // Peripheral Access Control Register
    AIPS_B.PACR[0].R    = 0x0;
    AIPS_B.PACR[1].R    = 0x0;
    AIPS_B.PACR[2].R    = 0x0;
    AIPS_B.PACR[3].R    = 0x0;
    //AIPS_A.PACR[4].R    = 0x0; - Reserved, not implemented
    AIPS_B.PACR[5].R    = 0x0;
    AIPS_B.PACR[6].R    = 0x0;
    AIPS_B.PACR[7].R    = 0x0;

    // Off-Platform Peripheral Access Control Register
    AIPS_B.OPACR[0].R = 0x0;
    AIPS_B.OPACR[1].R = 0x0;
    AIPS_B.OPACR[2].R = 0x0;
    AIPS_B.OPACR[3].R = 0x0;
    AIPS_B.OPACR[4].R = 0x0;
    AIPS_B.OPACR[5].R = 0x0;
    AIPS_B.OPACR[6].R = 0x0;
    AIPS_B.OPACR[7].R = 0x0;
    AIPS_B.OPACR[8].R = 0x0;
    AIPS_B.OPACR[9].R = 0x0;
    AIPS_B.OPACR[10].R = 0x0;
    AIPS_B.OPACR[11].R = 0x0;
    AIPS_B.OPACR[12].R = 0x0;
    AIPS_B.OPACR[13].R = 0x0;
}

ラベル(1)
タグ(1)
1 返信

1,668件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

The MPC5748G contains also the AIPS (peripheral bridge).

You can configure it in similar way as you see in the MPC5744P example.

It is well described in Reference manual:  3.6.1 Peripheral Bridge A memory mappastedImage_0.png

pastedImage_1.png

If want to access peripherals you need to grant access to them for particular masters exactly like in MPC5744P demo code.

Peter