Hi, first point is that you need to use right version of the example code
Example MPC5675K PinToggleStationery LSM CW210
Example MPC5675K PinToggleStationery DPM CW210
Second point is that MCU must be switched to particular mode.
If you use TRACE32 debugger (Lauterbach), attached script I made (...\t32\MPC5675K_switch_to_LSM_mode.cmm) changes the mode automatically (Power-on-reset) is required to finish to mode switch process.
If you are using PeMicro debugger, the process can be little bit more complex, see attached document describing is for CodeWarrior 10.x.
Also PeMicro has a solution for this operation: