Which is the best manner to configure the floating pins (MPC5607B)? Input pull-up or Output pull-up?

cancel
Showing results for 
Search instead for 
Did you mean: 

Which is the best manner to configure the floating pins (MPC5607B)? Input pull-up or Output pull-up?

208 Views
rafadelarosa
Contributor I

I am having some problems with the Quiescent current and I am thinking that maybe I have configured floating pins wrong.

Labels (1)
Tags (1)
1 Reply

74 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

For unused digital pins, it is recommended that software disable both the input buffers and the output buffers of the pads in the Pad Control Register for the pins. In addition, the weak pull-down device should be enabled.