Which document has a pin description about SPC5748C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which document has a pin description about SPC5748C

595 次查看
chenyandong
Contributor II

Hello,I want to extend the 2-channel Ethernet interface with spc5748c,but I can't see where I have a pin description on the datasheet.Can I extend two Ethernet interfaces?Which document has a PIN description?

0 项奖励
1 回复

410 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

See the device I/O Signal Description and Input Multiplexing tables attached to the device Reference Manual as

an Excel file (http://cache.nxp.com/assets/documents/data/en/reference-manuals/MPC5748GRM.pdf). Locate the paperclip symbol on the left side of the PDF window, and click it. Or open RM and press CTRL+SHIFT+A. Double-click the Excel file to open it.

Note: It is only possible to use ENET0 and ENET1 simultaneously when both are configured for MII_Lite.

BR, Petr

0 项奖励