Whether there is an I2C interface in MPC5777C?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether there is an I2C interface in MPC5777C?

ソリューションへジャンプ
1,080件の閲覧回数
chenyandong
Contributor II

I need an i2c interface to connect the temperature sensor.

NXP has a spi interface temperature sensor or not.

Another question,whether the eSCI interface can be configured as uart mode for RS232 or RS422.

Thank you.

0 件の賞賛
返信
1 解決策
911件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I2C module is not present with MPC5777C.

 

For connection of external sensor you may use DSPI module (recommended).

If I2C is necessary then you could possibly also use I2C function running on eTPU module (I would not recommend because number of required pins is doubled). Such function is provided by third-party provider:

https://www.ashware.com/i2c-driver

 

RS232/RS422/RS485 standard is given by version of physical layer connected to device externally, so yes, they can be used with MPC5777C’s eSCI interface.

元の投稿で解決策を見る

1 返信
912件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I2C module is not present with MPC5777C.

 

For connection of external sensor you may use DSPI module (recommended).

If I2C is necessary then you could possibly also use I2C function running on eTPU module (I would not recommend because number of required pins is doubled). Such function is provided by third-party provider:

https://www.ashware.com/i2c-driver

 

RS232/RS422/RS485 standard is given by version of physical layer connected to device externally, so yes, they can be used with MPC5777C’s eSCI interface.