Where can download the " SDK_S32_PA_15 " for MPC5744P Devkit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can download the " SDK_S32_PA_15 " for MPC5744P Devkit

Jump to solution
1,879 Views
Tod
Contributor I

Hi Sir 

I used the " MPC5744P REV_E Kit " and RTM3.0.0 , the SDK_S32_PA_11 included the FS65 component lib (SBC) inside. However , i updated S32DS_PA than this FS65 component lib was removed from SDK_S32_PA_11. Now, when I open this RTM3.0.3 example FS65 component lib that required to install the " SDK_S32_PA_15 " . 

Can you please help me to know where or how to download this " SDK_S32_PA_15 " and installing into S32DS_PA. 

Thank you and have a nice day

Todd 

0 Kudos
Reply
1 Solution
1,855 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is is part of 3.0.3 installation package.

petervlna_0-1674469924262.png

You simply select PA_15 and the project will be created.

petervlna_1-1674469977975.png

Best regards,

Peter

 

 

View solution in original post

0 Kudos
Reply
5 Replies
1,713 Views
rehab_hassan
Contributor II

rehab_hassan_0-1678697157942.png

 

rehab_hassan_1-1678697189118.png

 

 

 

0 Kudos
Reply
1,587 Views
Krishnayya29
Contributor I

Hi Rehab hassan,

Could you please tell me how can i resolve this issue because i am also not able to see

SDK_S32_PA_15 version .

 

 

Thanks,

Krishnayya

0 Kudos
Reply
1,713 Views
rehab_hassan
Contributor II

Hello, 

This window of selection doesn't appear with me and I have the same error, How could you solve it?

 

0 Kudos
Reply
1,856 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is is part of 3.0.3 installation package.

petervlna_0-1674469924262.png

You simply select PA_15 and the project will be created.

petervlna_1-1674469977975.png

Best regards,

Peter

 

 

0 Kudos
Reply
1,835 Views
Tod
Contributor I

Hello Peter 

I get it and find this PA15

Thank you and have a nice day 

Todd

0 Kudos
Reply