When manual reset/power off, the program is erased on MPC5748G-LCEVB!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When manual reset/power off, the program is erased on MPC5748G-LCEVB!

629 Views
keerthana_r
Contributor II

When I press a reset/power off switch on the MPC5748G-LCEVB, The program is erased and should flash manually again. I've flashed a basic "toggling a LED" code.

Is there any hardware or software configuration that I'm missing out ? 

0 Kudos
2 Replies

564 Views
F510223
Contributor I

Hi, have you solved the problem?

I am have the same issue when I press "flash" in the s32 studio the code runs, but is gone when reset/ power cycle.

 

0 Kudos

604 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

To me it looks like you does not load the code in the flash, rather then into RAM.

At leas the description looks like it.

Flash is not erased on reset, if the SW is not desired to do so.

Other possible explanation is that you see the SW only in the debugger, and it is not loaded in the chip.

 

best regards,

Peter

0 Kudos