What is the size of the SDM section in MPC5746R?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the size of the SDM section in MPC5746R?

434 Views
demian91
Contributor III

I have a problem what the initialization of eTPU when i reserve space in RAM memory. I understand that the SDM Memory is [0xFFCC8000, 0xFFCCBFFF]. But it crashed when i write in a position that after i could see in the IDE S32DS, the Memory Debug i try write 0xFFCC9800 because apparently the section [0xFFCC9800, 0xFFCCA000] of 2KB is not avaivable, i think is corrupted. Each write to the sector, it change all his values.

0 Kudos
1 Reply

413 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, there is 6kB of SDM memory used on this device

It means address range is 0xFFCC8000-0xFFCC97FF

davidtosenovjan_0-1639138319191.png

davidtosenovjan_1-1639138419665.png

But I agree it is no easy to understand it from this manual.

0 Kudos