What is the maximum SPI clock frequency in MPC5777C?

cancel
Showing results for 
Search instead for 
Did you mean: 

What is the maximum SPI clock frequency in MPC5777C?

Jump to solution
294 Views
shalakashinde
Contributor I

Hi,

I would like to know what is the maximum SPI SCK frequency in MPC5777C microcontroller.

I want to interface a WiFi module, which supports max SCK of 48MHz.

Thanks,

Shalaka

Labels (1)
0 Kudos
1 Solution
172 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, according specified SCK time, it is 30MHz (1/33ns)

pastedImage_1.png

View solution in original post

1 Reply
173 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, according specified SCK time, it is 30MHz (1/33ns)

pastedImage_1.png