What is Excute Access Control exception

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

What is Excute Access Control exception

413件の閲覧回数
reubenkim
Contributor II

I'm using MPC5746.

I met "Instuction Storage Interrupt (offset 0x30)" when the devince is in the high temperature.

The reference menual describes as below 

"An Instruction Storage interrupt (ISI) occurs when no higher priority exception exists and an Execute Access Control exception occurs."

Please let me know "Execute Access Control exception" and what can case this exception.

Thank you.

0 件の賞賛
3 返答(返信)

336件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, could you clarify used device? MPC5746B/C or MPC5746R? Thanks

0 件の賞賛

336件の閲覧回数
reubenkim
Contributor II

Hi, David.

It's MPC5746B.

Thank you.

0 件の賞賛

336件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

“Access control” is related to SMPU core exceptions that can lead in IVOR1/2/3 according table below:

pastedImage_1.png

I don't see any relationship with the temperature, if it is, then probably only random.

0 件の賞賛