Hi,
I am reading MPC 5748G microcontroller reference manual for FlexRay. I want to understand how to configure following given registers used for FlexRay FIFO message buffer configuration.
For Example my FIFO received ID's are,
The Frame ID for static slots is 0x02, 0x05, 0x08, 0x345, 0x415
The Frame ID for dynamic slots is 0x20, 0x30, 0x50, 0x100
The formula given for Static frame ID filtering is,
FID & FR_RFFIDRFMR[FIDRFMSK] != FR_RFFIDRFVR[FIDRFVAL] & FR_RFFIDRFMR[FIDRFMSK]
The formula given for Dyanamic frame ID filtering is,
MID & FR_RFMIDAFMR[MIDAFMSK] = FR_RFMIDAFMR[MIDAFVAL] & FR_RFMIDAFMR[MIDAFMSK]
Also please confirm the above highlighted register name. I think it should be FR_RFMIDAFVR[MIDAFVAL]
Solved! Go to Solution.
hi,
to make this simplier for you, there is an application note explaining FlexRAY, but it is not published officially yet.
In case you are interested in it please submit a case and I will sent it to you:
https://community.nxp.com/docs/DOC-329745
I cannot share it on community as it is not released.
regards,
Peter
Hi,
I am referring MPC 5748G microcontroller reference manual for FlexRay driver development.
With reference to below image,
The start byte address SADR_MBHF of each message buffer header field for the FIFO must fulfill Equation 16 on page 2193.
So for FIFO Do i need to refer Equation 16 or Equation 17. Also the Equation 18 when it will be used ?
Also Equation 17 or Equation 18 looks same.
hi,
to make this simplier for you, there is an application note explaining FlexRAY, but it is not published officially yet.
In case you are interested in it please submit a case and I will sent it to you:
https://community.nxp.com/docs/DOC-329745
I cannot share it on community as it is not released.
regards,
Peter
submitted the case. please share me application note. i will be much helpful while implementing a FlexRay driver.
Thanks !