Valid Censorship Passwords

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Valid Censorship Passwords

831件の閲覧回数
dpastl
Contributor II

Hello,

Is there any information on what a valid password is for use in censoring a device?  The Reference Manual for the MPC5674F states that a "valid password" should be programmed but I cannot find any mention of what "valid" entails. 

 

Certain flash passwords, generally ones with low values, do not appear to work correctly.  For instance a password of 0x1 will not allow the device to be accessed over JTAG.  Other passwords work just fine.  I can verify that both the control word and password are set correctly so I know it's not a problem with that.

 

Thanks!

ラベル(1)
タグ(1)
1 返信

631件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am not sure if reference manual mentions it somewhere or not but values 0x0000 and 0xFFFF cannot be used for Censorship Control Word (0x00FF_FDE0) or Serial Boot Control (0x00FF_FDE2).

Although I have found it described anywhere is the device’s RM, some related MCUs (for instance MPC5604B) has this restriction aslo specified for passwords:

When configuring the private password, each half word (16-bit) must contain at least one "1" and one "0".

I suppose it works same way for all MPC5xxx devices.