Using ENGCLK as 33 MHz Clock Source for External peripherals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using ENGCLK as 33 MHz Clock Source for External peripherals

1,909 Views
CNarendra
Contributor III

Hi @davidtosenovjan,

In our MPC5674F-based design, the system clock is configured at 264 MHz.
We require an additional 33 MHz clock for external peripherals but DCLK_OUT is already used elsewhere in the design.

We are considering using the ENGCLK pin for this purpose.

  1. Can ENGCLK be configured to output a 33 MHz clock suitable for external peripherals?

  2. Based on the reference manual, if we switch to an external 16 MHz crystal using the ECSS bit, is it possible to derive 33 MHz from ENGCLK?

    CNarendra_0-1753858485712.png

     

     

Thanks 
Narendra.C
MPC5674F 

Tags (1)
0 Kudos
Reply
3 Replies

1,900 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you can use it as you stated.

davidtosenovjan_0-1753871904676.png

 

0 Kudos
Reply

1,868 Views
CNarendra
Contributor III

hi @davidtosenovjan ,

Thanks for confirming.

Could you please share the manual or document where this block diagram is available?

Thanks
Narendra.C

MPC5674F 

Tags (1)
0 Kudos
Reply

1,845 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply