Unable to connect to MPC5675K

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to connect to MPC5675K

跳至解决方案
1,453 次查看
arun_mohanraj
Contributor II

we were trying to debug a working bare board project on a custom MPC5675 board.

After debugging and halting the device once, we were unable to connect the device any further.

The fowlling error had come

1 PASSWORD REQUIRED : Device may be censored. Please enter the password(in hex) to uncensor.

 

2 EPPC GDI protocol error: Failed to configure target. Processor configured as DPM/LSM opposite of the project settings.

 

We had attached the Diagnostic information

Original Attachment has been moved to: 201602241745_DiagnosticInfo.zip

标签 (1)
0 项奖励
1 解答
1,186 次查看
arun_mohanraj
Contributor II

FAB pin used for BAM was by default configured to Boot from inernal flash.

We had changed the configuration to boot from serial interface.

Then we are able to connect the debugger.

在原帖中查看解决方案

0 项奖励
2 回复数
1,187 次查看
arun_mohanraj
Contributor II

FAB pin used for BAM was by default configured to Boot from inernal flash.

We had changed the configuration to boot from serial interface.

Then we are able to connect the debugger.

0 项奖励
1,186 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

have you modified the shadow flash? It looks like the device is censored. In this case, it is possible establish the connection via JTAG in serial boot mode but it is not possible to read the flash content. Only first 16 bytes can be read around the RCHW address:

pastedImage_0.png

Could you check if you can read the flash memory in serial boot mode?

Regards,

Lukas

0 项奖励