USB TAP and codewarrior version (windows 8/10) for mpc5125 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB TAP and codewarrior version (windows 8/10) for mpc5125 processor

964件の閲覧回数
williammoreraro
Contributor I

Hi all,

 

         I am working on Twrmpc5125 processor. The USP TAP part number used for this is CWH-UTP-PPCC-HE. Now i need to flash this processor in windows 8 or 10. CodeWarrior USB TAP Vendor ID is 15a2, and the Product ID is 0319, Jungo WinDriver Version is 11.0. Could anyone tell me which CW version should i install that supports mpc5125 processor and can flash it with that USB TAP?

Thanks

タグ(1)
0 件の賞賛
返信
0 返答(返信)