Hello everyone,
I would like to consult one thing about TBG. My purpose is to trigger CFIFO with PIT periodically. I initialized MODE bits on CFCR register and ISEL registers. Also, As far as I understood, I have to initialize TBG to trigger CFIFO.
However, when I looked at the examples performed by NXP, I cannot see TBG registers.
Could you inform me what TBG is exactly?
Must I have initialize TBG for this purpose?
Sincerely.
解決済! 解決策の投稿を見る。
8.4.6 Trigger Burst Generators (TBG)
The TBG is in bypass out of reset, thus backwards compatible functionality is
provided. In this backwards compatible setting, the triggers are generated by the signals
connected to the IMUX, thus TBG is transparent to the trigger generation.
Tom
8.4.6 Trigger Burst Generators (TBG)
The TBG is in bypass out of reset, thus backwards compatible functionality is
provided. In this backwards compatible setting, the triggers are generated by the signals
connected to the IMUX, thus TBG is transparent to the trigger generation.
Tom