Timing accuracy of the MPC5674F PIT module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timing accuracy of the MPC5674F PIT module

Jump to solution
1,936 Views
youngseolee
Contributor III

I wanna know a timing accuracy of the MPC5674F built-in PIT module.

I downloaded a same SW to two development boards(Both boards have the same design) and measured a 10ms interrupt period generated by the PIT.
(When the PIT interrupt occurs, toggle I/O in the handler and measure the toggled I/O period using an oscilloscope)

For board 1, the interrupt period is measured to be within 0.01% of 10ms. On the other hand, for board 2, the interrupt period is measured to be within 0.02% of 10 ms.
There was a difference of about 0.01% in the PIT interrupt period error of the two boards.

I think that the difference in the PIT interrupt generation period between these two boards is caused by the accuracy of the used oscillator and PIT module (or FMPLL) .
(The oscillator we used has a precision of 0.005%)

We need accurate analysis, and for this we need the accuracy information of PIT module or FMPLL module. Can you let me know?

0 Kudos
Reply
1 Solution
1,890 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

A crystal driven PLL is phase and frequency locked on the crystal signal, thus retaining the crystal spec stability and accuracy in PPM. PLL output signal frequency accuracy expressed as +/-PPM deviation to the output target mean frequency is equal to the input target reference mean frequency. This is due to the PLL locking both phase and frequency to the input signal.

eMIOS/eTPU resolution is also given by source accuracy as possible dividers in the way does not change accuracy in ppm.

View solution in original post

0 Kudos
Reply
5 Replies
1,900 Views
youngseolee
Contributor III

So, what is the timing accuracy of the eMIOS timer (or eTPU)?

i'm curious about the accuracy of the built-in timer & FMPLL of the MPC5674F except for the oscillator accuracy.

0 Kudos
Reply
1,891 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

A crystal driven PLL is phase and frequency locked on the crystal signal, thus retaining the crystal spec stability and accuracy in PPM. PLL output signal frequency accuracy expressed as +/-PPM deviation to the output target mean frequency is equal to the input target reference mean frequency. This is due to the PLL locking both phase and frequency to the input signal.

eMIOS/eTPU resolution is also given by source accuracy as possible dividers in the way does not change accuracy in ppm.

0 Kudos
Reply
1,881 Views
youngseolee
Contributor III

Your answer helped me a lot. thank you.

0 Kudos
Reply
1,917 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

In your case I would see biggest issue with using PIT timer and so necessary ISR handling (may be affected by the core activity, active or pending interrupts and their priorities, XBAR latency and so).

Otherwise an accuracy is mainly given by oscillator accuracy. I would recommend to use eMIOS timer (or eTPU) to remove influence of the core.

0 Kudos
Reply
1,898 Views
youngseolee
Contributor III
Spoiler

So, what is the timing accuracy of the eMIOS timer (or eTPU)?

i'm curious about the accuracy of the built-in timer & FMPLL of the MPC5674F except for the oscillator accuracy.

0 Kudos
Reply