The project of lwip doesn't work in flash when reboot the board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The project of lwip doesn't work in flash when reboot the board.

1,360件の閲覧回数
lixu
Contributor II

Dear everyone,

I am using S32DS working on MPC5748G.

I am using the LWIP project in the example, and debugged it in Flash but every time I reboot it doesn't run .

I would like to ask what is the cause of this problem?

Thanks and best regards,

Li Xu

0 件の賞賛
返信
3 返答(返信)

1,148件の閲覧回数
jzhang
Contributor I

I met the same problem.  Have you found a solution?  Thanks!

Charlie

0 件の賞賛
返信

1,348件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

What do you mean by reboot? Reset the device?

What does it mean "it doesn't run" ? Is the device in reset, is the code in some exception? Or it is stuck waiting for some conditions?

best regards,

Peter

 

0 件の賞賛
返信

1,334件の閲覧回数
lixu
Contributor II

Hello,

I used the "LWIP" project in the example,I compiled this project into "Flash". When I reset the device,  There is no network transmission. (The way I think it is that after compiling into Flash, the project should be able to work ,whenever open the power supply.)

And I think it has a condition, because every time I compile, I need to press "resume" twice( Usually I think just press "resume" once. )

When I first hit "resume", it looked like this:

无标题.png

It didn't work until I hit "resume" a second time.

I want to know what should I do to make it work every time I turn on the power. 

best regards,

Li Xu

 

 

 

 

 

0 件の賞賛
返信