The correct result of the example hsm_freetos_mpc5748g

cancel
Showing results for 
Search instead for 
Did you mean: 

The correct result of the example hsm_freetos_mpc5748g

235 Views
961271210
Contributor I

I am trying to debug the example project hsm_freetos_mpc5748g on S32DS, although it does not have any problems and it can be download into my board, but after I download into my board, the board cannot give me any reaction. I would like to know what the correct result should be after the project being debugged? The project which I used is the example project which can be input from S32DS directly. 

Tags (2)
0 Kudos
2 Replies

130 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jupeng,

please do not use this example. There were some changes, this is not an option anymore and it will be removed.

To use HSM, it's necessary to order special part number at local sales office. This device will have HSM firmware programmed and you will get API and manual. It is not possible to place an order online. Standard part numbers like SPC5748G... do not have HSM firmware loaded, so HSM cannot be used (even if this standard part number suggests that HSM module is available). We have already asked to clear this up, I know it is confusing.

Sorry for inconvenience.

Regards,

Lukas

130 Views
961271210
Contributor I

Hi Lukas,

Ok, I get it........Thanks a lot. 

Jupeng

0 Kudos