The SJA1105 doesn`t woke well

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The SJA1105 doesn`t woke well

Jump to solution
1,456 Views
1693275120
Contributor II

HI

   My SJA1105T can`t work normal,i need some help. 

resolution.png

I had detect  signals at TXD[0:3]  from MCU to SWITCH, but i can`t detect signals at TXD[0:3] from SWITCH to PHY.

I had get some information from Software user manual for SJA1105TEL .

I read the  Initial device configuration flag register ,it shows the configuration is valid.

I read the  Ethernet high-level port status diagnostic counters part 1 ,the N_RXFRM  \N_RXFRMSH   \N_TXFRM\ N_TXFRMSH which show the tx/rx frames counter  is  always 0.
why?

0 Kudos
Reply
1 Solution
1,366 Views
bpe
NXP Employee
NXP Employee

If N_RXFRM doesn't change when you send traffic to the corresponding
port, it means the port is unable to detect a proper frame. This in
turn may happen due to wrong timing of the MII interface signals or
because the port is improperly or not fully configured. Suggestions:

1. Check error counters and flags described in UM10944, Section 5.1.4.1

2. Make sure CGU and ACU are properly configured for the used interface
   type. Note that this configuration is not part of the static configuration
   sequence. See AH1601 for more details, the document is available
   on Docstore.
  


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,367 Views
bpe
NXP Employee
NXP Employee

If N_RXFRM doesn't change when you send traffic to the corresponding
port, it means the port is unable to detect a proper frame. This in
turn may happen due to wrong timing of the MII interface signals or
because the port is improperly or not fully configured. Suggestions:

1. Check error counters and flags described in UM10944, Section 5.1.4.1

2. Make sure CGU and ACU are properly configured for the used interface
   type. Note that this configuration is not part of the static configuration
   sequence. See AH1601 for more details, the document is available
   on Docstore.
  


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,366 Views
1693275120
Contributor II
  1. I read the Section 5.1.4.1Ethernet port status - MAC-level diagnostic counters,the field N_SOFERR is0x04.

and the  Ethernet port status - diagnostic flags  is all 0, I don`t know what this means.

 

2.The static configuration sequence, I get from simpleT.py, and It's been modified a little bit to match my board

simpleT.png

speed.png

mac.png

  1. the CGU is configured like this, I had compared it with the corresponding part in AH1601, I am sure it`s right.

 

//MII CLOCK FOR PORT0 (PHY)
static const uint8_t port0_idiv0[] = {0x01|0x80,0x00,0x00,0xb0,0x0a,0x00,0x00,0x00};
static const uint8_t port0_mii_tx_clk[] = {0x01|0x80,0x00,0x01,0x30,0x11,0x00,0x08,0x00};
static const uint8_t port0_mii_rx_clk[] = {0x01|0x80,0x00,0x01,0x40,0x01,0x00,0x08,0x00};
static const uint8_t port0_ext_tx_clk[] = {0x01|0x80,0x00,0x01,0x80,0x11,0x00,0x08,0x00};
static const uint8_t port0_ext_rx_clk[] = {0x01|0x80,0x00,0x01,0x90,0x11,0x00,0x08,0x00};

 

//MII CLOCK FOR PORT1 (MAC)
static const uint8_t port1_idiv1[] = {0x01|0x80,0x00,0x00,0xc0,0x0a,0x00,0x00,0x01};
static const uint8_t port1_mii_tx_clk[] = {0x01|0x80,0x00,0x01,0xa0,0x02,0x00,0x08,0x00};
static const uint8_t port1_mii_rx_clk[] = {0x01|0x80,0x00,0x01,0xb0,0x03,0x00,0x08,0x00};

 

//MII CLOCK FOR PORT2 (MAC)
static const uint8_t port2_idiv2[] = {0x01|0x80,0x00,0x00,0xd0,0x0a,0x00,0x00,0x01};
static const uint8_t port2_mii_tx_clk[] = {0x01|0x80,0x00,0x02,0x10,0x04,0x00,0x08,0x00};
static const uint8_t port2_mii_rx_clk[] = {0x01|0x80,0x00,0x02,0x20,0x05,0x00,0x08,0x00};

 

//MII CLOCK FOR PORT0 (MAC)
static const uint8_t port3_idiv3[] = {0x01|0x80,0x00,0x00,0xe0,0x0a,0x00,0x00,0x01};
static const uint8_t port3_mii_tx_clk[] = {0x01|0x80,0x00,0x02,0x80,0x06,0x00,0x08,0x00};
static const uint8_t port3_mii_rx_clk[] = {0x01|0x80,0x00,0x02,0x90,0x07,0x00,0x08,0x00};

 

//MII CLOCK FOR PORT0 (MAC)
static const uint8_t port4_idiv4[] = {0x01|0x80,0x00,0x00,0xf0,0x0a,0x00,0x00,0x01};
static const uint8_t port4_mii_tx_clk[] = {0x01|0x80,0x00,0x02,0xf0,0x08,0x00,0x08,0x00};
static const uint8_t port4_mii_rx_clk[] = {0x01|0x80,0x00,0x03,0x00,0x09,0x00,0x08,0x00};

 

4.The ACU part

/* Configure CFG_PAD_MII0_RX[CLK_IPUD], Pull down MII0_RX_ER */
static uint8_t tmp[8] = {0x01|0x80,0x00,0x80,0x10,0x02,0x02,0x03,0x12};

 

If you find any problems,i will really appreciate.

0 Kudos
Reply