The pin that controls LED3 in the SAMPLE given by AUTOSAR_OS is what GPIO100 says in the instructions
I think it should be controlled with other pins, such as the encapsulated pin 45 of the controller (GPIO39/PC[7]) and why is LED3 defined as
#define LED3 2 Why do you define the installation package this way
MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3 folder
Hi,
the example is obviously written for this board:
... where LED3 is connected to PG4 pin:
PG4 is GPIO100:
So, I can see no problem here.
Regards,
Lukas