The FlexCAN configuration in MPC5606/SPC5606

cancel
Showing results for 
Search instead for 
Did you mean: 

The FlexCAN configuration in MPC5606/SPC5606

Jump to solution
752 Views
ycgxy1650601
Contributor III

hi:

The MCU(MPC5606/SPC5606) has six FlexCAN modules. Every FlexCAN module can be configured to the high speed mode or low speed mode,is right ? According to the document(SPC5606B Microcontroller Reference Manual).

thanks

1 Solution
699 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, FlexCAN module has full Implementation of the CAN protocol specification, Version 2.0B and has programmable bit rate as fast as 1 Mbit/s.

BR, Petr

View solution in original post

1 Reply
700 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, FlexCAN module has full Implementation of the CAN protocol specification, Version 2.0B and has programmable bit rate as fast as 1 Mbit/s.

BR, Petr